I am having an issue with the PCA9306 not working correctly when I turn on an unrelated power supply.
I am translating between 1.8V to a voltage that will vary between 3.2V and 4.2V. My design pretty much mimics Figure 7 from the datasheet. I also have 2.2k pull-ups on the 1.8V side located elsewhere on the schematic. My schematic is attached below:
The PCA9306 works perfectly when the unrelated power supply is off. Enable and VREF2 are stable and are at a decent voltage level. See scope capture below (Blue- En / VREF2, Yellow - SDA):
When the power supply is turned on and the current ramps up, the En / VREF2 start to behaving erratically. See scope capture below (Blue- En / VREF2):
En / VREF2 have dropped from approximately 3.6V down to minimum of 1.3V. En / VREF2 start to droop more and more until the PCA9306 turns off and the SCL and SDA lines stop toggling I have tried different capacitance on En / VREF2 from 1000pF to 0.1uF. I have also tried changing the resistor from 50k to 300k. The scope capture above is with a 50k. From the schematic above, BAT_4002, 1.8V, and gnd are all stable and not fluctuating.
Why would turning on an unrelated power supply affect the performance of the PCA9306 especially when all the rails provided to the PCA9306 are stable?
Thanks,
Tyler