Hello,
In our design we used sn65hvd78 ic for one way data transmission between subsystems. A subsystem pcb has one data receive part and one data transmit part on it. Those parts have sn65hvd78 ics that are set to receive and transmit modes. Subsytems are connected with cat5 cable with each other. By that way we planned to send data over subsystems. The cat5 cable only have data+ and data- differential pairs, no ground is going over cat5. Common ground is only at power supply parts of the subsystems.
We have many subsystems that are mounted to a large area. One subsystem's average current consumption is about 3A. More than 10 subsystems are powered with a uniqe power supply.
Our problem is that sometimes the data communication fails. When we investigate the problem, we saw that the sn65hvd68 at transmit part of subsytem pcbs is damaged and not working. So data communication fails. We think that the reason of failure is ground loop since there is no isolation in send or receive parts of pcbs.
We have two options. One option is adding some componenets to pcb so that the isolation will be assured. The other option is to replace sn65hvd78 with an isolated differential line driver.
Could you provide a solution to us?
Could you also suggest an isolated differential driver for 10mbit data rate?