Dear all.
Is this device supporting L-Line?
Regards,
PAN-M
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear all.
Is this device supporting L-Line?
Regards,
PAN-M
Hi PAN-M,
Did you mean to type "K-Line" which is a ISO 9141 standard? If so, the SN65HVDA195-Q1 is the correct device to use for this application since K-line supports data rates down to 10baud (100ms/bit). The SN65HVDA195-Q1 does not have a dominant state timeout feature built in, so it can support data rates down to DC.
The main difference that you should be aware of is that typically in K-line the pull-up resistor is external to the device and is on the order of 200kΩ. Since the SN65HVDA195-Q1 was derived from a LIN transceiver, it has a built in pull-up resistors on the order of 20kΩ-60kΩ with a series blocking diode.
Please let me know if you have any other questions.
Thanks,
John
Thank you for answer, John-san.
This question from our customer.
We thought that we had to know a standard more from your reply.
Thanks and Regards,
PAN-M