Hi,
I have a question about CAN tranceiver product.
I'm searching CAN tranceiver for DeviceNet and found SN65HVD251D CAN Tranceiver.
Is it available to use SN65HVD251D for DeviceNet?
best regards,
g.f.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi G.F.
The DeviceNet standard is a higher-layer protocol that was developed by Allen Bradley that works on top of the CAN physical layer. While I do not have a copy of the standard since it is only available to DeviceNet members at http://www.odva.org/ I have seen the following list of requirements before. I went through the HVD251 datasheet and made a quick comparison for you.
Parameter
|
DeviceNet Specification | HVD251 |
Number of nodes | 64 | yes |
Minimum differential input resistance | 20 kOhms | 40kΩ |
Minimum differential input capacitance | 24 pF | 20pF Typ |
Bus pin voltage range (survivable) | -25V to +18V | ±36V |
Bus pin voltage range (operation) | -5V to +10V | -7V to +12V |
Differential output voltage | 1.5V with 50 Ohm load | 2V min @ 60Ω |
Maximum transmitter propagation delay | 80 ns | 150ns max for full transceiver loop delay (both parts added) |
Maximum receiver propagation delay | 90 ns | 150ns max for full transceiver loop delay (both parts added) |
Receiver hysteresis | 150 mV (spec’d as typ) | 100mV Typ |
Transmitter output current limiting | internally limited | yes |
Please let me know if you have any questions.
Thanks,
John
Hi John,
Thank you so much for the reply.
So, it seems that HVD251 matches DeviceNet Specification except propagation delay,
and I understood as that HVD251 can be use for DeviceNet.
By the way, I found from the HVD251 datasheet that DeviceNet was written as
feature of HVD251. So, it's supporting DeviceNet.
best regards,
g.f.