I would like to use the SN6501 to generate a +/- 20V isolated supply that I will regulate down to lower voltages. The data sheet shows examples of ways to generate higher output voltages. Figure 48 in the data sheet shows how to generate a high voltage bipolar supply, but I think there might be an issue if the positive and negative outputs are not equally loaded. The other examples are OK because they are either full-wave or unipolar. The problem with half-wave bipolar is that one transistor of the SN6501 ends up driving the positive supply, and the other transistor drives the negative supply. Won't this cause a core magnetization issue because of the imbalance? If so, how much imbalance would be acceptable? I will be using the 1:2 Wurth transformer and a 5V supply for the SN6501.
Thanks,
Greg