Hello,
I have been using SN65HVD485 on my control boards without issue, on my new control board I need to be able to hot plug the connectors, I tried to use the SN65HVD1785 as a direct replacement but I cannot get it to work. The master is an AB MV169e-MBS. I have 20 slave control boards per system.The received signal output is less than 2V in amplitude.