Hello, is it possible to damage CAN transceiver chip SN65HVD1050 by inducing a 75 kV potential into it then collapsing it several times? I have parts with EOS damage and one of the failure modes is overvoltage for long periods of time. I do not have this specific scenario, but I could have the potential for statically induced voltage up to 75 kV, which can be induced and collapsed many times over a relatively small period of time.