Part Number: DS26C32AM
Dear forum:
Please see the attached sketch which is the reference for my questions. I am using a DS26C32 RS-422 differential receiver in an application in which I desire to support both RS-422 inputs and TTL inputs. Circuit 1 shows the classic differential DC termination. This works well for RS-422, has higher DC dissipation and would not support TTL inputs. Circuit 2 uses an AC differential termination and works OK with zero DC dissipation but would not support TTL very well.
In my third approach, I use a split AC termination that looks to the transmitter like nearly 120 ohms for transitions and provides some filtering of noise. The #A circuit is for RS-422 with A and B inputs while the 3B circuit uses the 10k/6.8k bias string to set the inverting input of the receiver near 2V, A TTL input applied to the positive input with respect to ground see some input filtering but not a low value DC termination. In my view this approach should work well in both applications.
Are there any potential problems with my circuit 3 approach for RS-422 and TTL support?
Thanks