Other Parts Discussed in Thread: STRIKE
Hi,
I was wondering how to protect (if needed) a fault protected CAN transceiver (TCAN1051HV).
The datasheet says CAN lines are protected up to +/-70V (short to battery). This is great.
I was wondering how to design line termination and ESD (ISO 10605, 25KV) protection circuit to survive to such shorts as well.
For instance, TCAN1051HV is not protected up to ISO10605 25KV, or is it?
ISO7367 or ISO16750 pulse 5b (load dump with centralized load dump suppression) for example, battery voltage can rise up to 65V in 10ms rise time, and pulse duration is about 400ms.
With this specs, TCAN1051HV can survive such voltage, but the problem is how to design the line termination and ESD protection so they can also survive to such shorts.
Regarding line termination, I guess this is not only to properly size the resistor, as 120R resistor with 65V across terminals will dissipate near 35W... Even 24V short means 4.8W...
And regarding ESD, any usual ESD TVS diode won't withstand a load dump pulse...
Any help would be greatily appreciated! Thanks,
Carlos