Hi Support,
1. As the end user won’t know or care about which node is the first node and last node in RS-485 network if they are 32 nodes.
Is that possible to communize all resistor value for every node?
2. MCU 3.3V and SN65176B 5V
MCU UART TX connects to D of SN65176B shall be OK
MCU UART RX connects to R of SN65176B we are not sure if the high-level output voltage damage MCU I/O as the MAX value below is not defined.
Thanks.