Tool/software: TINA-TI or Spice Models
Hi,
I need to replace an old rheostat from the 1930s that is no longer made. It contains asbestos, so it can't be shipped and repaired.
I was thinking that if I could build a variable duty cycle square wave generator, it would have the same effect as the rheostat. I'd then run that output through an Op-Amp and to an SCR, and it would control the 250 V dc 300 Amp circuit.
Does TI make a square wave generator with a frequency set by selection of a capacitor and the duty cycle set variable from 0% to 100% by a variable resistor?
Thanks.
Sincerely,
Del Ventruella