Hello All,
My customer has the below two questions on the Fault Protection feature of the SN65HVD1781 Device:
1) What is the maximum DC voltage that can be applied between A and B bus pins without damaging the part?
2) What is the maximum AC voltage that can be applied between A and B bus pins without damaging the part?
From what I can see from the datasheet it looks like the fault protection is for voltages applied between one bus pin (A or B) and GND or VCC, but doesn't say anything about protection from voltages applied directly between pin A and B.
Thank you!
Best regards,
Mo.