What's the max multiple transceivers number?
Cant find on spec, pls help.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Piero,
The SN65HVD72 has a receiver input current of 150 µA at 12 V. It is a 3/20 UL(Unit Load) transceiver, and no more than 213 transceivers should be connected to the bus.
-Lucas