Hi all,
Since i am new to CAN protocol i have the following doubts during my study, could anyone help me to understand the queries.
1. Why dominant bit has high priority in CAN protocol?
2. Is it possible to assign same CAN ID for two messages? If yes, then how does the arbitration handle for this?
3. If data and remote frame with same message ID and start transmit at same time which frame(data or remote) win the bus?
4. The nodes connected in the bus have different baud rates, how does the synchronization happened?
5. How can calculate the time taken to transmit a CAN message with 11 bit identifier at 512 kbps?
6. How does the uC get to know whether the received bit is dominant or recessive?
Thanks in advance