This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MAX3222: Capacitor rated

Part Number: MAX3222

Hello,

Our customer use the MAX3222, have a question.

There are four capacitors for charge pump circuit.

How much the voltage rated for?

Could you give me the equivalent circuit of the charge pump?

Best Regards,

Naoki Aoyama

  • Naoki,

    The voltage rating for the external capacitors should be at least as high as 10V or higher like 16V.

    Please find equivalent charge pump circuit as below. The mechanism is that C1 and C3 transfer the charge to generate 2 times Vcc on V+, then C2 and C4 copy this voltage to V- with reverse polarity. 

    Please let me know if you have any more questions.

    Regards,

    Hao

  • Hello,

    Thank you for your reply.
    I will feedback the customer this information.

    Thanks,
    Naoki Aoyama