Part Number: TUSB3210
Dear Mr./Mrs.,
I want to use TUSB3210 with double buffering of USB.
At "TUSB3210 usb firmware programming flow 8052",the toggle bit of the OEP seems to be automatically set (toggled) by UBM after ISR is returned. is that correct?
And then the UBM for OEP seems to receive next packet on new toggle bit indexed buffer only if the NAK bit of that buffer is cleared.
If the NAK bit of the next buffer (indexed by toggle bit) is still set, do the UBM search the other buffer with NAK bit cleared or wait for the NAK bit cleared?
By the way, in the IEP, the toggle bit seems to be set by software in interrupt service routine (ISR) after the CTX is cleared NAK. is that right?
Thanks
Cheolhyeon Cho