Other Parts Discussed in Thread: SN74LVC245A
We are using TXB0104PWR level translator in one of our custom board to shift SPI(Serial Peripheral Interfac) pins.Following is the snapshots of the schematics related to TxB0104PWR IC.
The issue is that after using this level shifter SPI logic zero is geting boosted up to 0.8V to 1 V but we are expecting the ouput from level shifter logic zero to be 0V.
Pease help us to resolve this issue any help would be greatly apreciated.
Thanks & Regards
Brijender