Hi. Team.
There is no "Ioh" indication while examining the TXB0104 specification.
I want to know the "Ioh" specification of TXB0104.
Can you check it?
Thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi. Team.
There is no "Ioh" indication while examining the TXB0104 specification.
I want to know the "Ioh" specification of TXB0104.
Can you check it?
Thanks.
Hi
Thank you for your reply.
But I want to know the range of Min / Typ / Max, not Max Ioh.
Is it possible to check?
Thanks.
Best Regards,
The output current is not determined by the TXB; it depends on the load you put on the output.
The minimum IOH is 0 A, when nothing is connected to the output.
The typical IOH is the actual leakage current of whatever input you have connected to the output. (The 20 µA limit implies that you must connect a CMOS input.)