Other Parts Discussed in Thread: TX517,
Hello,
We are still looking for a method to change the output frequency of TX517EVM to 400Khz or 800Khz. By default, the buttons on the board generate a signal between 5 MHz to 100MHz. This frequency is appropriate for medical applications. However, our application is sonar. Is there any method to change the frequency? Would it be possible to control this board externally?
We were thinking to generate PWM wave using our OMAP L138 LCDK, and then give this PWM wave as input to TX517EVM . Then TX517EVM would generate the output frequency based on the PWM that we gave TX517EVM as input. However, I don't know if it's possible or not.
Any suggestions or advice is appreciated.