Other Parts Discussed in Thread: TXB0304, TXB0302
Hi All,
I am using the TXB0106 Voltage level translator to interface with LE910 module.
I have a query on the VOL and VOH levels of the translator.
For more understanding, I am attaching the Image over here
I am supplying VCCA = 1.8V and VCCB = 3.3V.
As you can see from the above Image VOLA =0.4V (max) @ –40°C to 85°C but my module LE910 can accept max 0.35V. Is it work or Creates any problem @ 0°C to 50°C?? What is the value of VOLA max @ 0°C to 50°C ??
Same for the VOHA = 1.4V min @ –40°C to 85°C but my module LE910 can accept min 1.5V. Is it work or Creates any problem @ 0°C to 50°C?? What is the value of VOLH min @ 0°C to 50°C ??