Hi
I have some question about enabling and disabling by EN.
On the datasheet at section 10, it is mentioned as below.
[The outputs are into a high-impedance state when the EN pin is pulled to low.]
However at section 8.4, it is mentioned as below,
[The I/Os will be disable and pulled to Vcca, Vccb through 40kohm.]
Which is it correct? Or Does the high-impedance mean 40kohm?
Regards,
Koji Hamamoto