Other Parts Discussed in Thread: SN74AXC8T245
We used TXS0108ERGYR in our design
But we found that the TXS0108ERGYR only supports data rates up to 60MHz, which means that the clock signal only supports 30 MHz transmission.
However, we use up to 48MHz clock signal transmission in our design.
Please help us find the level shifter that satisfies our conditions
- Pin to pin with TXS0108ERGYR
- Has an OE input that is used to disable the device by setting OE low, which places all I/Os in the Hi-Z state.
- Data rates supports up to 100MHz.