This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ISO1042-Q1: CAN and RS485 Isolation hardware review

Part Number: ISO1042-Q1

Hi TI team,

Please find the attached schematic of CAN and RS485 Isolation circuit including Power isolation for them and kindly review the same.

CAN-Isolator.pdf

One major concern here is can it be possible for TPS76350QDBVRQ1" LDO to drive both CAN and RS485 Isolators and 2 mmore digital Isolators are also there in my design?

I don't think so because LDO output current is 150mA, So Please suggest a LDO with lower dropout voltage, because LDO input will also be 5V appr.

Please check the circuit and support on this part ASAP.

Thanks

Manjunath