In the data sheet, SCES296AC-FEBRUARY 2000-REVISED APRIL 2014, is table 6.2 Thermal information. But header of the table states SN74LVC1G00. Is table information for 1G00 or 1G07?
Paragraph 9.2 Typical Application shows Wired OR schematic. But it is wired AND!
In paragraph 11.2 Layout Example shows unused inputs connection, but 1G07 has only one input! Or the example applies to NC pin 1?
There are too many inaccuracies in this document. How much can I trust information in it?
Can I write or talk directly to application engineer?