I have an application where on onside of the LSF0102YZTR is a micro-controller which will be programmed to communicate i2c or SPI master the other side will be either i2c or spi slave. The micro-controller will be 3.3 connected to the "b" side of LSF0102YZTR. the "a" side will be vddio = 3.3 - 1.2V. pin 7 & 8 are connected to 3.3v through a 200Kohm resistor. Pins 3 &4 are pull up independently with 332 ohm resistor to vddio
Will there be any issues with using this part in "spi mode"
thanks!