Dear Team:
Our customer used SN74LVC1G07, but got seems gound bound at output, when Power off.
As below is their circuit and waveform. Second 2 picture is Zoom in picture.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear Team:
Our customer used SN74LVC1G07, but got seems gound bound at output, when Power off.
As below is their circuit and waveform. Second 2 picture is Zoom in picture.
Sorry, I overlooked these labels.
The Ioff feature of this device works when the power is switched off. However, the power supply for this device is P3V3_STBY, which stays up.
Switching off P3V3 affects only the input signal, and with the slow decay shown above, the input signal violates the input transition fall time (Δt/Δv in table 6.3 of the SN74LVC1G07 datasheet). Oscillations are expected to happen when you do that; see Implications of Slow or Floating CMOS Inputs (SCBA004).
You should connect the buffer to the power supply that is always switched off first. If that is not possible, use a buffer with a Schmitt-trigger input (e.g., SN74LVC1G17, with a push/pull output).