Other Parts Discussed in Thread: SN74LVC1G34, SN74LVC3G34, SN74LVC2G34
Hi
I was wondering if it is possible to use the TCA9800 in parallel with "push pull" outputs, to supply "additional" current to charge capacitive loading.
I have a SIM card interface with excessive capacitive loading on it. I had intended using the TCA9800 (B side) to provide the additional current to the
bidirectional Open drain I/O as mentioned before in a previous "post". I need to add large Pull down resistors on the on the B side of the TCA9800 due to possible floating pin issues.
I am aware that the values of the pull downs need to such that Iext-i and Iext-o are not exceeded (something in the order of 50K is required)
The SIM card signals may be at either 1.8V or 3V levels.
I have similar capacitive loading issues on the RST and CLK push pull output lines (from the modem to the SIM card) of the SIM card interface. So I was wondering once more if I could use the TCA9800 to supply the additional current to charge these capacitive loads .
Maybe there is a better solution from TI to do this. I need to drive capacitive loads in the order of 200pF. The input signals (from the modem card interface) can be either 1.8V or 3V levels. There is a negotiation phase between the modem and the SIM card which determines what the signal levels will be. I need to meet 1us rise and fall times.
If you have nay queries let me know.
Finbarr Long