Need advice selecting a logic family. Requirements:
* Through hole parts.
* Standard 74xx devices readily available.
* As fast as possible using 2-layer boards.
* Power draw not important.
Application: Custom CPU.
Leaning towards ACT.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Need advice selecting a logic family. Requirements:
* Through hole parts.
* Standard 74xx devices readily available.
* As fast as possible using 2-layer boards.
* Power draw not important.
Application: Custom CPU.
Leaning towards ACT.
Ok, so even with the slower HCT in DIP, the main speed limitation would be board layout?
My understanding is ACT is 10X faster than HCT.
Are you saying that it wouldn't help improve speed of the circuit?
If that's true, why would a selling point of ACT be speed if it couldn't be used?
I'm not trying to be practical on this project and just throw in an off-the-shelf MCU, reasoning is for all my other projects :)
If you pull up datasheets for a D Flip-Flop from each family (I chose the 374 function), at 5 V the HC device is rated to ~60 MHz (typical) operation, and the ACT is rated to ~160 MHz (typical) operation.
What you're talking about isn't using one or even just a few devices (which is usually how these devices are used), you're talking about using hundreds of them in conjunction, with many inputs tied together and traces/wires running everywhere (a CPU is pretty complex, as I'm sure you know). I would be surprised if you could get a discrete computer running past 1 MHz. I have seen some similar builds in the past, and they typically operate in the low kHz range.
The speed of the device will certainly make a difference in many applications, but in this one, you will run into many other bottlenecks. I wish you luck in this project -- it's a big undertaking!
If you want to see a more direct comparison of ACT and HC, you can check out or Logic Guide, page 11 has some details on both families listed out.