Hi, I am looking to use either the SN74AVC32T245ZKER in a test fixture and I was wondering if you could clarify on the switching speeds for 1.8V to 3.3V level translation.
SN74AVC32T245ZKER promises a 1.8V to 3.3V level translation at 380 Mbps. I am not certain if this means 11.875 MHz x 32 bits or 380 MHz switching speed. All test numbers show 10 MHz and below.
Can you clarify on the maximum switching speed on this part?
Thanks!