Dear team,
My customer wants to know below questions, could you please help answer? Because they need to compute thesystem's total Ioff which exceeds the requirements now. Their VCC is 5V.
what is the max Ioff when the temperature is 25°C ?
what is the max Ioff when the temperature is 85°C ?
In our datasheet, Ioff's max value is 10uA. What is the test temperature? It should be at the 125°C ,right?
Thanks & Best Regards,
Sherry