Hi,
I have questions related to the Hercules mcu (TMS570LS2125).
Could you answer the following questions?
1. When I don't connect FLTP1, FLTP2 and TEST termination, what do the terminations work?
I wonder if no connect (NC) occurs the bad influences.
2. When the VCC (1.2V) terminations and the nPORRST termination are shorted, what will happen?
Does the reset circuits will never be activated by the nPORRST termination?
3. When the VCCP termination and the VSS (GND) terminations are shorted, what will happen?
And in the above case, what does the cpu behave?
I wonder if the flash and the mcu work safety.
thanks
Nomoto