I have a large screen and tired eyes so I am using the 125% Font Size in Windows. Looks like the editing controls do not align with the rest of UI in this case?
Is this a known issue? if it is not, what is the best way to report it?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I have a large screen and tired eyes so I am using the 125% Font Size in Windows. Looks like the editing controls do not align with the rest of UI in this case?
Is this a known issue? if it is not, what is the best way to report it?
Hi Andrey,
This is a known issue. HALCoGen does not support enlarged Windows fonts. The background in the GUI is a static picture which does not scale up with higher font size.
Thanks and Regards,
Vineeth
Good to know that you are aware of the issue. Are there any plans to address it?
I would assume that if you insist on the sizes defined in the image you should be able to locate the editor controls at the hard-coded coordinates.