Dear all,
I am trying to remap the interrupt priority. I build a project and enable 2 interrupt sources, (rtiCompare0Interrupt, etpwm1Interrupt)
The frequency of rtiCompare0Interrupt is 1Hz. The counter is RTICRT.
The frequency of etpwm1Interrupt is 1MHz. The counter is PWMCRT.
When I use default setting for interrupt priority, the test result is normally. I run the program about 7 sec.
However, when I remap the priority, No.2<->No.90,
the test result show only 1 Hz interrupt request in the two counters.
In my opinion, RTICRT should change to 1MHz, and PWMCRT should change to 1Hz.
Could you help solve my confuse? Also I attach my project as follow.