Hi.
I would like to know whether there are possibilities to protect the code on the TMS570 MCUs? And if there are then how it can be done? The code protection that I am talking about basically concerns the code read-back once the devices flash is programmed. We would like to prevent the read-back of the code. For example our current systems implement code protection in a way where after the firmware is programmed and verified the read-back is prevented by reading out all 0x00 values. However, new programming of the memory is still possible (meaning it is not permanently locked). Does TMS570 offer similar functionality? We require this to protect our firmware against unauthorized copying.
We will program the MCU via JTAG connector and are planning to use Segger Flasher PRO device for the task.