All,
This the the kind of question I hate when users ask, because they should be able to find the information without asking, but I have run into a number of windows only roadblocks, so I need help. (and apologize in advance)
I am new to ARM processors/microcontrollers, but have 20 years plus with x86 C/asm programming. My dear brother, a long time TI EE sent me the RM46x (RM46L852) board and I have downloaded CCS, and built/run project 0. Board connects fine with the XDS 110 driver, but I was unable to complete project 0 (without downloading the finished project files from the wiki) because there is no HalCoGen for Linux, etc. (why we are using gio to twiddle bits is another question -- for later)
Since many of the tools HalCogen, uniflash, etc. are windows only and I have no windows, I would like to understand how to work from LInux alone. I am used to coding with vi and xterm, calling gcc directly. What I would like to find is a link or two that discuss the command line tools available to (compile, link, erase flash, program flash, run, etc) without having to touch an IDE. The eclipse/CCS tool is fine, just really cumbersome to someone used to running from the command line.
Is there are link (or collection of links) that provide an overview and short howto on the necessary command line tools used to accomplish what CCS does without CCS? Obviously CCS does it, and I could probably just make individual calls to the various parts of CCS, but that seems like overkill just to cross-compile, erase and program the flash memory. I have both the TI compiler and gcc-arm compilers installed. Any links or suggested reading on this topic would be appreciated.