Hi Team,
Recently, we have procured TMS570LS3137ZWT and started testing HET module using Code composer Studio 6.2 version.
Test case: We have configured in such a way that for pin 30 in N2HET1 module, a square wave of 3 volts peak to peak is applied with 32 KhZ. We have configured N2HET1 such that if the input frequency <=33 Khz, pin 31 should be set.
L06 MCMP { next=L09,en_pin_action=ON,cond_addr=L07,pin=31,order=REG_GE_DATA,action=SET,reg=R,data=0x1C};
But, we could see that PIN 31 is always SET irrespective of whether the magnitude comparision is satisfied or not satisfied.
Please confirm, is it the expected behavior?
Note: We are using the Evaluation board.
A quick response is highly appreciated.
Regards,
M.Sreenivasan.