Part Number: RM48L930
Hello,
My project requires floating point support, and the uC I am using (RM48L930) contains a FPU coprocessor. In the HALCoGen 'Cortex R4 - General Configuration' area I enabled "Enable Vectored Floating Point Unit". However, I don't see a call to _coreEnableVfp_() in sys_startup.c. Is this a known issue in HALCOGen 4.07.00? Do I need to add a call to _coreEnableVfp_() to enable the FPU coprocessor? My project compiler processor options are set to -mv7R4 --float_support=VFPv3D16.
Thank you,
Keith