Part Number: TIDM-TMS570BMS
Hi Guys,
I'm using EM1402EVM together with LAUNCHXL-TMS57004 to perform active balancing. I'm able to balance current (charge and discharge) at 5A.
I want to balance the cell at current 10A or more for battery 16s cell in series(total cells voltage = 60V).
Based on the EMB1499Q datasheet, the balancing current can be set as below:
Ibalancing = Vsense_hs / Rsense
Set Vset = 2.2V
Vsense_hs = Vset / 40 = 0.055V
Let say, I want to set Ibalancing = 10A
So I change the Rsense = 0.055 / 10 = 5.5mohm to achieve 10A balancing current right. Beside changing Rsense, what else components need to modify?
Thanks,
Regards,
XH Low