Hi,
I am using msp430f6736. I configured the sd24 adc with OSR = 256, left aligned, offset binary.. clocked with 1MHz and using internal 1.2V reference. I connected both SDP0 and SDN0 to ground and started conversion for converter 0. The converter converts but results are not correct. According to datasheet, for above mentioned configuration the values should be SD24BMEMH0 (=0x8000) and SD24BMEML0 (=0x0000). But I am getting other values than. Any help with be appreciated.