Hello!
As the title said I want to operate the Launchpad MSP430FR5969 @ 1,8V supply voltage. However it first starts to work @ 1,9V. That's very unfavourable when you want to use a linear regulatar to power the board. In the forum is already another thread http://e2e.ti.com/support/microcontrollers/msp430/f/166/t/282823.aspx with the same topic but without a real solution for the problem. Because the thread was started in august 2013 i hope there is a solution now. As I understand from the datasheet I have to change the SVS levels. But after reading the users guide it doesn't seem to be possible.
Thanks for your help!
Simon