Trying to compile the examples for the MSP430FR5969 Launch Pad and SHARP display..
Having successfully built the other two example, the 430BOOST-SHARP96_ULP_FRAM_16KB example fails..
I am using a 'free' install of the CCS and compiler, so the 16K limit is the max size, as I understand(?) things.. and as such I chose this version to build.. however I get link errors related to mismatched memory models..
I am using factory make files, etc.. -- any ideas what I need to do here ?
-- there are 22 errors - 0ne is shown ---------------------------
'Building target: 430BOOST-SHARP96_ULP_FRAM_16KB.out'
'Invoking: MSP430 Linker'
"C:/TexasInstruments/ccsv6/tools/compiler/msp430_4.3.3/bin/cl430" -vmspx --abi=eabi --data_model=restricted -O4 --opt_for_speed=0 --advice:power="none" --advice:hw_config=1 -g --gcc --define=__MSP430FR5969__ --diag_warning=225 --display_error_number --diag_wrap=off --silicon_errata=CPU21 --silicon_errata=CPU22 --silicon_errata=CPU40 --printf_support=minimal -z -m"430BOOST-SHARP96_ULP_FRAM_16KB.map" --heap_size=160 --stack_size=160 --use_hw_mpy=F5 --cinit_hold_wdt=on -i"C:/TexasInstruments/ccsv6/ccs_base/msp430/include" -i"C:/TexasInstruments/ccsv6/tools/compiler/msp430_4.3.3/lib" -i"C:/TexasInstruments/ccsv6/tools/compiler/msp430_4.3.3/include" -i"C:/TexasInstruments/ccsv6/ccs_base/msp430/lib/5xx_6xx_FRxx" -i"C:/TexasInstruments/ccsv6/ccs_base/msp430/lib/FR59xx" --reread_libs --priority --warn_sections --display_error_number --diag_wrap=off --xml_link_info="430BOOST-SHARP96_ULP_FRAM_16KB_linkInfo.xml" --rom_model -o "430BOOST-SHARP96_ULP_FRAM_16KB.out" "./ActivePowerMeasure.obj" "./ClockApp.obj" "./FR59xx_EXP.obj" "./FRAMSpeedApp.obj" "./Game.obj" "./ULPMeter.obj" "./msp430fr59xx_CHR.obj" "./myTimer.obj" "./grlib/Sharp96x96utils.obj" "./grlib/sharp96x96.obj" "../430BOOST-SHARP96_ULP_FRAM_Lib.lib" "../lnk_msp430fr5969.cmd" -l"libc.a" -l"libmath.a"
<Linking>
error #16019-D: file "../430BOOST-SHARP96_ULP_FRAM_Lib.lib<adc12_b.obj>" specifies small data memory model, which is not compatible with restricted large data memory model specified in a previous file or on the command line