We are currently using the MSP430F5529 chip with our prototype. There is an issue with the USB drawing current when it is not in use.
Before USB was enabled, the board would draw 80 uA of current. After calling the function USB_setup(TRUE, TRUE) at start up the board would draw 209 uA while in low power. I fixed this by only calling the setup function after the USB was plugged in. But after it is unplugged, it starts drawing the 209 uA again.
So I tried calling these functions when the USB is disconnected:
USB_reset();
USB_disable();
USB_setEnabledEvents(0x0000);
USB_disconnect();
However, the device still draws 209 uA so it seems like this is not successfully disabling the USB. So my question is, how do you successfully reverse the current draw caused by the function USB_setup(TRUE, TRUE)?
For quick reference, here is the current draw for the different scenarios mentioned:
1. USB not enabled at all: 80 uA
2. USB enabled at beginning of program: 209 uA
3. USB only enabled after it is plugged in: 80 uA (before plugged in) -> 209 uA (after being plugged in and then unplugged)