I've been trying to get the USB serial port on the Launchpad working for a while now with no success. I have been reviewing all of the forum postings and any other internet information I can find. But nothing has helped so far.
I am just trying to use the port to read back live data from an MSP430G2553 as a debugging aid.
This is where I am:
- I am Using Windows 8.1 and have the CCS development suite loaded
- I have confirmed that the TI USB serial port driver is loaded. Under Ports in Device Manager I see MSP430 Application UART (COM3). It shows "working properly" and I have the parameters set to 9600-N-8-1 with no flow control.
- I have a modified version of the UART echo character sample project loaded into the 2553 that just sends out upper and lower case A-Z in an infinite loop. I have confirmed with a scope that I am getting serial data out of the TXD pin on the 2553. The timing/character length looks about right for 9600 baud. One bit is about 104 uSec.
- I'm using a Rev 1.5 Launch pad and I've also confirmed with a scope that I'm seeing serial data at R6 - BRXDI on U1.
- I've opened the COM port in Putty and in the Terminal window in CCS. I see nothing. No characters, no garbage, just nothing. In Putty, if I try typing characters I see nothing on the TXD side of U1. If I set Putty for Local Echo I can see what I'm typing. But nothing seems to be transmitting.
When I have the port open in the terminal window of CCS, if I try typing anything, CCS locks up completely and I have to close it.
I am out of ideas. If anyone has any suggestions, I would greatly appreciate it.
Thanks,
Tom