Hello
I am a question on the boot loader:
I have designed a boot loader and splitter MSP430 memory image into 2 parts: main image and secondary image.
I am using interrupt jump table to re-direct CPU to jump between images.
The image arrives from the air.
I see that write an image correctly yet the following is a problem:
I am using IAR toolchain and compile with short data model.
The image I send is the one from the output of IAR when compile using map-txt format
What I have noticed is that the TXT file received from IAR and the image read back after i download using IAR are different at some bytes...The difference is at the are of functions __data16_memcpy and other system functions.
Why there is a difference between the TXT file and the image file downloaded from IAR?
This is urgent issue so appreciate a quick reply.
Thanks