I've been using the MSP430G launchpad with mspgcc and mspdebug for a while now, and it forms a very comfortable development environment.
However, I now need some more RAM, so I've ordered the FR5969 based Launchpad. Unfortunately, I now see that mspgcc comes with a big warning that if I use it this will brick the device.
The bug seems to date from last year, and hasn't been fixed yet. Plus the mailing lists haven't shown much activity this year and the project looks suspiciously dead.
I also see that there's a gcc available from TI, but I've yet to successfully make it work (TIs binary downloads don't work for me, so I'll have to build it from source... ugh). The source, however, looks like it doesn't come with mspdebug.
One of the reasons I'm using the msp430 is because the Unix development environment was so nice, so this is all kind of a disappointment...
Does anyone know:
(a) if TI's compiler is safe to use on the FR5969?
(b) whether it works with the stock mspdebug (version 0.22-2, apparently)? And whether it's safe? And if mspdebug is deprecated, what the alternative is?