Hi all, Am programming MSP430G2553 via BSL using MSP430F5438.
These are the BSL commands working fine
1.RX password
2.Mass erase
3.TX data block
and below are the commands am not able to execute. Getting checksum error(NACK). I am able to send header,data and when i try to send checksum data, it gives NACK. The Checksum code is same here which i used for above commands.(Mass erase)
1.RX data block
2.Erase check
3.TX BSL version
there are other commands also but i have not checked them.
So any solution???