Hi,
I'm looking for PCB design guidelines when creating PCB with MSP430's. I was hoping there is a literature on this somewhere.
Thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I'm looking for PCB design guidelines when creating PCB with MSP430's. I was hoping there is a literature on this somewhere.
Thanks.
co tang87699 said:when creating PCB with MSP430's
Hi some guidelines are present about low power xtal to avoid noise and possible refuse to start at all.
About HF xtal some care must be done to isolate from external noise too and is mandatory if USB is present. Some cap as usual on pcb must be very close to power pin...
But forever missing detail which one of huge family?
USB or not, if RF require more close rules due to RF impedance match an as RF in general too...
Analog require have less noise.. Analog are different and many resolution/architecture span the family...
So which device or subfamily?
Application specific guidelines?
PCB is an art, it must be done with knowledge or thing doesn't work.
What answer do you expect?
PCB should be using proper electrical design for everything and a mcu don't have special rules that only apply to it.
1: Use star (tree branch) pattern for Vdd and Vss
2: Don't run digital traces under the crystal
3: Protect the mcu from brownout with a inductor(or resistor) and a bulk cap
4: Use a Ferrite Bead on Avdd, if the mcu have separate analog power input.
co tang87699 said:Well, I came across a stellaris guideline that was very well informed.
Uhm.. also old prematurely dead Stellaris was split across family to different chip if USB analog ENET or peripheral .. if you need general guideline ok but for PCB yes there are some application notes about crystal and specific one..
MSP is different from Stellaris now TIVA and require different PCB routing rules. Rules come from application type, Stellaris has no differential high resolution AD, MSP is more complex or more simple.. Which one and what application?
Jens-Michael Gross said:And of course, when using a layout program, don't place all bypass capacitors in one corner because it is so easy to route. (don't laugh, have seen people doing it. I have even seen it in diagrams.).
Hi Jens, this is politically incorrect, you cannot write this good novel than disable laugh free... Ok I have seen a lot of these and also when all seems ok some strange interaction move current flow away from where we think has to be. Solid planes are the more confounding from where rf energy find conduction path.
PCB designing is an art and need be learned day by day from guide, experience and good friends. I think guidelines not specific from stellaris are still good for MSP, some examples can be found on devkit or special layout recommendation on MSP specific folder.
I wish you all the best for your day.
co tang87699 said:Is there not a single general guideline when designing PCB's with MSP430s
I searched for a document I was inspecting some time ago, try if this can help you, all hardware are described and schematic and some guideline are present.
http://www.ti.com/general/docs/lit/getliterature.tsp?baseLiteratureNumber=slau278&fileType=pdf
**Attention** This is a public forum