i am using msp430g2553 Ic. not launchpad. and i want to make Pc based acqusition system can you tell me how to do it? mY uart pin is p1.1 and p1.2
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
i am using msp430g2553 Ic. not launchpad. and i want to make Pc based acqusition system can you tell me how to do it? mY uart pin is p1.1 and p1.2
ok thanks. i have one question: when i am using USB to TTL converter with launchpad, i connect its tx and rx pins to rx and tx pin of launchpad. it works for me. but when i am not using launchpad, then how to connect usb to ttl converter with msp430g2553??
it is not working for me. when i check connection using multimeter, in MSP430 side rxd pin is connected to p1.3 and txd is not connected to p1.2 and on emulation side first pin is connected to p1.2
Remember to connect GND of your circuit to the GND of the converter. Also ensure if Tx/Rx of the converter refers to the side of PC or side of your circuit. You can do it fast using multimeter - check where voltage changes when you send data via PC terminal - this pin shall be connected to MSP430's Rx pin. Some converters also requires to choose if you want to use 3.3V or 5V (requires removing jumper etc.).
Best regards,
Mikolaj
**Attention** This is a public forum