I have connected the MSP430-BSL to a MSP430G2553 as follow:
BSL MSP430G2553
Pin1 Pin 3 - P1.1
Pin3 Pin 7 - P1.5
Pin 4 Pin 16 - RST
Pin 5 Pin 20 - GND
Pin 6 Pin 1 - VCC
Pin 7 Pin 17 - TST
I attempted to use the BSLDEMO2 program to connected to the device but the synchronization fails every time.
I then used teraterm set the bit rate to 9601 baud and this does instigate to BSL entry sequence.
Is it possible to use the BSL-Scripter with value line devices or am I going to have to write my own tool?
Any suggests would be a great help.