Hi,
I have got the mmc.c sorted to be used with the SDHC card. the writing on the SD card is happening at 4 MHz, I need help and suggestions on the following:
1. How do I write the SDHC card in FATFS. I have gone through the elm-chan FATFS but am stuck as to how do i integrate the various commands with that of mmc.c
2. How do I make the card write at a higher speed. I have tried 2 cards and with of them if I increase the clock speed the card does not respond back with R1 command when I send CMD0. Instead the MISO line is always showing 0xFF at speeds higher than 4 MHz
Regards
Viney Chaddha